AnsweredAssumed Answered

Are ADC1/2/3 in the F103 totally inedpendent?

Question asked by c.a.001 on Aug 24, 2013
Hi there,
    If I setup both ADC1 and ADC2 in independent mode and set ADC1 to scan channels 1,2,3 using DMA and setup ADC2 for analog watchdog on channel 2 having different sampling times for channel 2 between the two ADCs.  Would ADC1 and ADC2 be operating totally independently having absolutely no effect between the two ADCs?  ie, if both ADCs happen to want to sample channel 2 at the same time, would one has to wait for the other?  or worst corrupt the other's sample, etc...?

Outcomes