AnsweredAssumed Answered

strange current consumption

Question asked by ml.michal on Jul 21, 2013
Latest reply on Jul 21, 2013 by ml.michal
Hi All,

i have issue with current on STM32F417 (100pins) :-(

when i connect power and BOOT0 is set to run into STM's bootloader i have power consumption 88mA,
and when i jump into my program i have 120mA :-(
i have connected but not initialized ULPI interface and other peripherals,
peripherals that are working correctly and was tested are
USART1, USART6, SPI3, and some GPIOs,
could you help me please how to identify where is something wrong ?

Thanks for all replies,

Outcomes