AnsweredAssumed Answered

SPI on Medium-density devices

Question asked by cronin.tom on Jul 18, 2013
Latest reply on Jul 18, 2013 by Clive One
I am using the STM32L151RBH6 which I believe is a medium density device, I am trying to get SPI working using the STM32Lxx_spi.c library but from reading the header at the top of V1.1.1 the I2S feature is not working for my device.
My questions are:
1) Is the V1.1.1 the latest peripheral library?
2) If I cannot use the SPI_I2S_SendData() command is my only option using DMA or writing my own driver? Does anyone know if DMA SPI works on medium density devices
Thanks
Tom

Outcomes