AnsweredAssumed Answered

STM32F427 - USART - most significant bits problem

Question asked by ClementGrosjean on Jul 17, 2013
Latest reply on Jul 18, 2013 by ClementGrosjean
Hello,

I'm trying to make a communication protocol via the UART. I have a M4 and an A8 which communicates via RS485 transmitters.
For the trials, the UART is set to 9600 bps, 8 bits per character with one stop bit and an even parity, but I regularly get an error at the reception, the most significant bit is forced to one.
I checked the frequency, it is of 9615 Hz to the transmition on both microcontrollers. And in the example code I saw that the most significant bit was filtered. (I think it is for reception of a character of the ASCII table)

this is the reception in ST's example code :
 /* Read one byte from the receive data register */
    aRxBuffer[uhRxCounter++] = (USART_ReceiveData(EVAL_COM1) & 0x7F);

regards,

Outcomes