AnsweredAssumed Answered

Embedded SRAM as the boot space

In AN2606 it's described when both BOOT0 and BOOT1 are pulled-up, Embedded SRAM is selected as the boot space.

How can I load my application to SRAM without programming FLASH and run it after loading without any reset?

Flash Loader Demonstrator has an option for Jump to the user program but the drop-down box to set address is not changeable and fixed on @ (h) 8000000.

Regards مانیتورینگ اتوماسیون صنعتی طراحی توسعه سیستم مخابرات شبکه امنیت کنترل پروژه الکترونیک میکروکنترلر

Outcomes