AnsweredAssumed Answered

Using TIM9 for PWM input

Question asked by michael.tamir on Jul 3, 2013
Latest reply on Jul 3, 2013 by waclawek.jan
Which IRQ do I need to use ? I don't see any IRQ related to TIM9 at stm32f4xx_it.h.
TIM8 can also do PWM input - which IRQ do I need to use there ?

void TIM8_BRK_TIM12_IRQHandler(void);       /* TIM8 Break and TIM12 */
void TIM8_UP_TIM13_IRQHandler(void);        /* TIM8 Update and TIM13 */
void TIM8_TRG_COM_TIM14_IRQHandler(void);   /* TIM8 Trigger and Commutation and TIM14 */
void TIM8_CC_IRQHandler(void);              /* TIM8 Capture Compare */

Thanks in advance

Outcomes