AnsweredAssumed Answered

speed of Tim8 vs. Tim4

Question asked by ml.michal on Jul 3, 2013
Latest reply on Jul 3, 2013 by ml.michal
Hi all,

i'm using STM32F407 with 12MHz ext. crystal with 168MHz system clock, i use demo for STM32F4Discovery,

i configured Timer4 and Timer8 in same way,
specifically: ARR=1, PSC=0, CKD=0,
and i'm measuring 42MHz on both timers,
is it something worng configured ?
Timer8 is on APB2 so it should be twice faster than Timer4 , shouldn't be ?

please help me to understand,

Kind regards,

Outcomes