AnsweredAssumed Answered

How start running STM32 firmware from IROM2 ?

Question asked by khodarahmi.ehsan on Jul 1, 2013
Latest reply on Jul 1, 2013 by Clive One
I'm developing an embedded application using Keil MicroVision 4 & STM32F103RE
I've splited Flash memory of device into two areas (IROM1 & IROM2) using IDE target options panel (Target tab, Read only memory areas section) & also setted IROM2 as default & startup, but seems the program does NOT run from specified address.
Should I do anything more than told configurations to start running program from an address rather than FLASH_BASE (0x08000000 in my case)?

Outcomes