AnsweredAssumed Answered

STM32F105/107 HID USB device SET_REPORT, GET_REPORT

Question asked by ioakim.stelios on Jun 21, 2013
Latest reply on Mar 13, 2015 by chang.cheng_huan
Dear all,

I am using the "STM32_USB-Host-Device_Lib_V2.1.0", which I think is the only one that fully supports the STM32f105/107 OTG functionality and has a Custom HID demo project, to add USB functionality on my design. I am trying to make the device be recognized as an HID device for input AND output meaning that I want to control my device over a computer software that I've already implemented and successfully used with an STM32F103 series microcontroller.

Unfortunately, the library that was used to implement the embedded software on the STM32F103 does not work with the STM32F105 one and the one that works ("STM32_USB-Host-Device_Lib_V2.1.0") has only IN functionality implemented.

What I am asking for here is if someone has used the STM32F105 to implement both IN and OUT functionality on their design and which library they've used to do it. Basically the library that I am using now is missing the GET_REPORT function and has only the SEND_REPORT.

Thanks,
Stelios

Outcomes