AnsweredAssumed Answered

FSMC with Display, Ram & Flash possible?

Question asked by Emilio on Jun 10, 2013
Latest reply on Jun 10, 2013 by Clive One
Hi,

is it possible to use this two or three Devices on the FSMC or what is the max of possbile peripherials on the FSMC bus?
I wanted to connect my Display and an external SRAM (like the one of the STM32 Eval Board) with the LQFP176pin STM32F427.
My TFT: SSD1289 (http://www.wvshare.com/product/3.2inch-320x240-Touch-LCD-A.htm)

In the Microexplorer would I choose FSMC_CF for the display and FSMC_NOR_RAM for the SRAM?

Kind regards
Emilio

Outcomes