AnsweredAssumed Answered

Image file httpfsupdate maximum size

Question asked by catherall.paul on Sep 2, 2016
Latest reply on Sep 2, 2016 by Gerardo Gallucci
Hello
I am using a Nucleo F103 RB with XNUCLEO-IDW01M1 board to develop the code.

I have been successfully using the Update over the air feature for some time.
I now have an image file that has grown because of the extra features on the Web pages etc

From my console I get the following message :-

<TX> at+s.httpdfsupdate=192.168.0.12,/outfile.img
<RX>  Invalid HTTPD_FS image, length (633215)

I am not sure if my image file is somehow corrupt or just too large.
My previous image files have worked perfectly from a PC set up as web server
and are approx 300k in length.
I have tried running Httpd_gen.exe a few times but the same results. 
Is there a maximum size permitted ?





Outcomes