AnsweredAssumed Answered

Typos in Reference Manuals for STM32F3

Question asked by gary on Jun 5, 2013
Latest reply on Jun 19, 2013 by Amel N
 st.mcu told me to report on this forum any corrections needed in reference docs and code.

These corrections apply to the latest published reference manuals for STM32F3xx:

                                               
           
RM0316: STM32F302xx, STM32F303xx and STM32F313xx advanced ARM-based 32-bit MCUs DM00043574.pdf
           
DocID 022558 Rev 2.0
                                               
           
RM0313: STM32F37xx and STM32F38xx advanced ARM-based 32-bit MCUs DM00041563.pdf
           
DocID 022448 Rev 1.0

1) Table 24. Programmable data width & endian behavior; Source port width=32, Destination port width=16: Transfer operations should read "WRITE BxBy[15:0]" not "...[7:0]"

2) USART Section 5.4 Baud rate generation; Example 1 In case of oversampling by 8: calculation should read "0x3 >> 1" not "... << 1".

-Gary

Outcomes