AnsweredAssumed Answered

spwf01 module Timing Issue

Question asked by goudra.basavanagouda on Sep 1, 2016
Latest reply on Sep 28, 2016 by schrader.kale.001

Hi,

 

I observed followings while communicating between two spwf01modules:

 

       
  •    

    At    the Client side when its try to connect to server I’m using AT+S.SOCKON command    to connect.

       
  •    
  •    

    In    this command I can pass “ind” parameter which can indicate data arrival at the    client side with “+WIND:55:Pending Data” on UART interrupt .

       
  •    
  •    

    Client    side it is taking 500ms to receive WIND:55:Pending Data: interrupt.

       
  •    
  •    

    Server    to client data transmission it takes only 5 to 6ms.

       

     

       

Please suggest how to solve this time delay at the client side.

 

Thank you

Basavanagouda

Outcomes