AnsweredAssumed Answered

STEVAL-IHM022V1

Question asked by Machfax on May 10, 2013
Hi

I'm interesting to use the STEVAL-IHM022V1 Evaluation Board to drive 2 BLDC DC Motors from Maxon with Encoder and HallFeedback (3pole 24VDC 40W). I need to drive them in sine modulation with the FOC control.
Now which power stage board should I use? Is there some evalaution board from ST to use?
The other question I have is the positioning mode. I need to drive the moltor with a speed x to the position y. Is this part implemented in the STM32 Dual FOC MC Software library?

Regards, Dominik

Outcomes