AnsweredAssumed Answered

What RAM types can i use in STM32F4 100-pin packages?

Question asked by marques.pedro.002 on Apr 30, 2013
Latest reply on Apr 30, 2013 by jj.sprague
Hello,

after reading and reviewing 1 dozen times the RM and app notes, i could not come to a clear conclusion on what type of RAM i can use in STM32F4 100-pin packages. The more clear and detailed info was for NOR flash and NAND flash but no certains about PSRAM or SRAM, even being stated in the RM as being possible to use them in multiplexed mode.
Can i really use PSRAM or SRAM chips with 100-pin packages? If so, the PSRAM/SRAM chip should be specific (i'm asking this because i looked the specs of a bunch of them and i never found any kind of NADV line, i suppose, needed for multiplexing)? Is there any example i can check?

Outcomes