AnsweredAssumed Answered

DfuSe Demo crashes during Verify

Question asked by edlund.mattias on Apr 19, 2013
Latest reply on May 23, 2016 by Toby
Hi,

I'm trying to use the DfuSe Demo (v3.0.3) to program the STM32 on an STM3240G-EVAL board. When I click "Upgrade" in the tool it works as long as I do not select "Verify after download" or click the "Verify" button.

I'm running 64-bit Windows 7 Proffessional.

When I click "Verify", the Dfuse Demo application crashes and a "DfuSe Demo has stopped working" dialog is displayed with the following detailed information:
----------
Problem signature:
  Problem Event Name:     APPCRASH
  Application Name:     DfuSeDemo.exe
  Application Version:     3.0.3.0
  Application Timestamp:     4ecd2975
  Fault Module Name:     StackHash_427e
  Fault Module Version:     6.1.7601.17725
  Fault Module Timestamp:     4ec49b8f
  Exception Code:     c0000374
  Exception Offset:     000ce6c3
  OS Version:     6.1.7601.2.1.0.256.48
  Locale ID:     1053
  Additional Information 1:     427e
  Additional Information 2:     427e33db81e067f5c132bd61e44036e8
  Additional Information 3:     dfff
  Additional Information 4:     dfff3649a8f15f879c998a2d67599592
----------

I desperately need to be able to upgrade device firmware over USB.

What can I do to make this work?

/Mattias

Outcomes