AnsweredAssumed Answered

USB and CAN STM32F

Question asked by dimitrov.valentin on Apr 19, 2013
Latest reply on Apr 20, 2013 by Clive One
In the RM0090 Rev.3 there is a note in the CAN section saying
"Note: In low, medium-, high- and XL-density devices the USB and CAN share a dedicated 512-byte SRAM memory for data transmission and reception, and so they cannot be used  concurrently (the shared SRAM is accessed through CAN and USB exclusively). The USB  and CAN can be used in the same application but not at the same time."

In the RM0090 v4 the note is missing. 
so I'm not sure if I can use the USB and CAN1 at the same time on STM32F405 ?!?

Outcomes