AnsweredAssumed Answered

STM32F4 AND ENCODERS

Question asked by s.esat on Apr 15, 2013
Latest reply on Apr 15, 2013 by Clive One
Hello friends
I am confused where to wire my encoders to stm32f4 ; I have 2 encoders from 2 motors ,
After I read the manual is it possible to wire the 2 encoders to the same timer and can configure them individually ? or I need two timers ?
for example encoder 1 A to timer2 ch1 and B to timerch2
encoder 2 A to timer2 ch3 and B to ch4 (timer 2)
is that ok ? Or do  I need 2 seperate timers ?
Do you suggest a direct wirring of the endoders or should I use latches?

Thank you in advanced .
Esat

Outcomes