AnsweredAssumed Answered

BootLoader with AN2557 creat bin file

Question asked by strauss.bar on Mar 25, 2013
Latest reply on Mar 25, 2013 by Clive One
For the demo example AN2557
1.does it need a special bin file to creat, because standard bin file doesn't contain the format show in the YMODEM.c ?
2.Does this format made by the UART modem if put in YMODEM?
3.What is the porpose of all the files locate in binary folder under IAP example? I try to operate the hex2bin.exe but no window open.
4. Does standard bin file also contain location index or just raw data? And if it just raw data it is mean that I have to put it byte after byte start from the file reset point? DOes it also mean taht if there a gup in the address I get lines of 0x00 or 0xff at that place?
Reagrds
Bar.

Outcomes