AnsweredAssumed Answered

STMStudio 3.1.1 does not show all variables on import

Question asked by Tobias on Mar 13, 2013
Latest reply on Jul 1, 2013 by S C
Hi,

after I updated the STMStudio I'm not able to import all variables from the .efl file.
After selecting a file there are not all variables shown. I tried different toolchains, but the problem is still there.

I use an old config (I think it was created with STMStudio 2.x or something) and my charts and variables are working.
I can also add new variables to the "Display Variables settings" but I must do this by hand:
1. Right click "new", rename it  to my variable name
2. Looking for the address of the variable in .map file or disassembled source.
2. Set the corect address and type.

Now I can use it as before for example in graphs or tables.

I'm not sure if I did something wrong, but the variables are present in .map and also in .elf file (checked with an text editor).

Has somebody a suggestion for me?

Thanks and greets
Tobias

Outcomes