AnsweredAssumed Answered

STM32F100 UART Transmission with Interrupt mode

Question asked by Mahabir Prasad on Feb 23, 2013
Latest reply on Feb 23, 2013 by Clive One
I am using STM32F100CB in my application. I am also using the example code
of UART Interrupt. The Receiver section is OK. For Transmission by interrupt.
I do not understand how to start 1st byte. (In 8051, used like prepare the buffer for tx, set all the pointers and index etc), either set the TI bit or copy the 1st byte in SBUF to start the transmission, in end of TX interrupt, ignore the tx interrupt).
Can you some hint similar manner for STM32F.

Outcomes