AnsweredAssumed Answered

I'm having some problem with Virtual EEPROM API with STM32F MCU

Question asked by lee.jongheon.001 on Feb 1, 2013
Latest reply on Feb 4, 2013 by lee.jongheon.001
When the virtual eeprom api function is erasing a page, it interrupts systick interrupt.
I toggled a led on every 100us to check systick interrupt in alive, but when the api function start to erase a page(for example 0x08030000), there are no interrupt untill it finishes(it was take around 30ms)
It is normal or there are someting else that interrupts the systick interrupt?

Outcomes