AnsweredAssumed Answered

Data transfer between two STM32 devices using FSMC

Question asked by Ferreira on Jan 26, 2013
Latest reply on Jan 28, 2013 by Ferreira
Hi,

I'm currious if it is possible to share data between two STM32 devices, using the FSMC interface.
Is it possible to configure one device as a Master and the other as a slave and use the FSMC? I would make the slave device act, as it was a SRAM memory, for example.

If not, is there a parallel peripheral to transfer data between two STM32 devices?

Thanks in advance,

Regards,

A. Paiva

Outcomes