AnsweredAssumed Answered

STM3221G-EVAL Keil uVision SDIO

Question asked by lewandowski.zbigniew on Jan 10, 2013
Latest reply on Jan 11, 2013 by lewandowski.zbigniew
Hello,
I'm using:  STM3221G-EVAL board with Keil uVision V4.53.0.0 and supplied by MCD Application Team SDIO_uSDCard example software V1.1.0 to test operation of  SDIO and micro SD card on the evaluation board. STM32F217G is selected and ST-Link debugger. All options for Target are working OK with different software examples. With the SDIO_uSDCard example I can not programm.
The error pops: Error Flash Download Failed -'Cortex-M3' and after OK compiling and linking I got:
Program Size: Code=7236 RO-data=484 RW-data=76 ZI-data=104660
".\STM322xG_EVAL\STM322xG_EVAL.axf" - 0 Error(s), 0 Warning(s).
Load "C:\\P556\\STM32F2xx_StdPeriph_Lib_V1.1.0\\Project\\STM32F2xx_StdPeriph_Template_SDIO\\MDK-ARM\\STM322xG_EVAL\\STM322xG_EVAL.AXF"
Full Chip Erase Done.
No Algorithm found for: 08000000H - 08001E73H
Programming skipped!
What is wrong? 
JP16 and JP22 is 1<->2

Outcomes