AnsweredAssumed Answered

PWM Time shifting signal

Question asked by waytae on Jan 9, 2013
Latest reply on Jan 15, 2013 by mendes.ari.001
Hi,

I program a PWM signal in PB4 port using TIM3 using this program

int main (void)
{
while(1)
{
TIM3->CCR1 = 1000 ;        
}
}
 
/*____________________________TIM3______________________________*/
  /* TIM3 clock enable */
  RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE);
  /* GPIOB Clock  */
  RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE);
 
  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4 | GPIO_Pin_5 | GPIO_Pin_0 | GPIO_Pin_1;
  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP ;
  GPIO_Init(GPIOB, &GPIO_InitStructure);
 
  GPIO_PinAFConfig(GPIOB, GPIO_PinSource4, GPIO_AF_TIM3);
  GPIO_PinAFConfig(GPIOB, GPIO_PinSource5, GPIO_AF_TIM3);
  GPIO_PinAFConfig(GPIOB, GPIO_PinSource0, GPIO_AF_TIM3);
  GPIO_PinAFConfig(GPIOB, GPIO_PinSource1, GPIO_AF_TIM3);
//________________________________________________________________
/*__________________________TIM3____________________________________*/
 
  /* Time base configuration */
  TIM_TimeBaseStructure.TIM_Period = 1999;
  TIM_TimeBaseStructure.TIM_Prescaler = PrescalerValue;
  TIM_TimeBaseStructure.TIM_ClockDivision = 0;
  TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
  TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure);
 
  /* PWM1 Mode configuration: Channel1 */
  TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;
  TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
  TIM_OCInitStructure.TIM_Pulse = 0;
  TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
  TIM_OC1Init(TIM3, &TIM_OCInitStructure);
  TIM_OC1PreloadConfig(TIM3, TIM_OCPreload_Enable);
 
  /* PWM1 Mode configuration: Channel2 */
  TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
  TIM_OCInitStructure.TIM_Pulse = 0;
  TIM_OC2Init(TIM3, &TIM_OCInitStructure);
  TIM_OC2PreloadConfig(TIM3, TIM_OCPreload_Enable);
 
  /* PWM1 Mode configuration: Channel3 */
  TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
  TIM_OCInitStructure.TIM_Pulse = 0;
  TIM_OC3Init(TIM3, &TIM_OCInitStructure);
  TIM_OC3PreloadConfig(TIM3, TIM_OCPreload_Enable);
 
  /* PWM1 Mode configuration: Channel4 */
  TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
  TIM_OCInitStructure.TIM_Pulse = 0;
  TIM_OC4Init(TIM3, &TIM_OCInitStructure);
  TIM_OC4PreloadConfig(TIM3, TIM_OCPreload_Enable);
  TIM_ARRPreloadConfig(TIM3, ENABLE);
 
 
  /* TIM3 enable counter */
  TIM_Cmd(TIM3, ENABLE);
//________________________________________________________________


It gives a PWM with 50% Duty Cycle

I want to shift time of this signal like this

images.jpeg

I have already Signal 1 i want to create Signal 2 shifted by period T

sigops1.png

What parameter have i to change ?

i try to change

  TIM_TimeBaseStructure.TIM_ClockDivision = 0;

from 0 to 1 the signal change but i don't understand the ClockDivision   effect

What is the ClockDivision
  interval variation to shift signal ?

Thanks

Thank you

Outcomes