AnsweredAssumed Answered

internal CAN bootloader in connectivity line devices

Question asked by QuirinoColombani on Jan 8, 2013
I would like to test the built in bootloader of the STM32F105VC using the CAN bus to make sure it (the bootloader) could be used in our product. I was wondering if anyone here could support me with a program, which could be used to flash the uC through CAN. I've got an ESD CAN-USB/2 but a program using an API different to ESD's would also be of great value - it would greatly shorten our prototyping process.

Outcomes