AnsweredAssumed Answered

STM32F4xx TIM7 Stopping

Question asked by kasapoglu.orkun on Jan 4, 2013
Latest reply on Jan 4, 2013 by kasapoglu.orkun
I want to use TIM6 and TIM7 together .

TIM6- Update Event - 2MHz  priority 0x10
TIM7- Update Event - 1MHz priority 0x00

when I closed TIM6 , TIM7 is running normally and toggling LED from PD14 but when I enabled TIM6's CEN bit TIM7 is stopping.
I'm sending the project. Thanks.

Attachments

Outcomes