AnsweredAssumed Answered

F37x documentation inconsistency--comparator port B

Question asked by haselwood.don on Oct 8, 2012
Latest reply on Oct 17, 2012 by haselwood.don
Which to believe--

STM32F32x datasheet (Sept, Doc ID 022691):
Page 40, Table 15, Alternate functions for port PB, shows COMP1_OUT and COMP2_OUT for AF8 on PB8 and PB9.  Table 14, port PA, shows PA0/PA6/PA11 and PA2/PA7/PA12.  (Table 13, pin definitions, is also consistent with Tables 13 & 14.)

Ref Manual (RM0313, Sept, Doc ID 022448 Rev 1):
Page 276, fig 51, shows only PA0/PA6/PA11 and PA2/PA7/PA12, with no mention of the port B pins.

My guess is that the datasheet is more likely correct than the ref manual.  I don't want to get too far down the road with the design and find that my guess was wrong.  (Maybe this is why it is called the f3-Discovery board--one needs it to discover how the part really works...)

Don

Outcomes