AnsweredAssumed Answered

IAP for STM32F0

Question asked by thieu.toan on Oct 8, 2012
Latest reply on Dec 22, 2015 by Clive One
Dear Friends,
I read document AN4065 of ST. it told that use must configure 2 conditions for application code, I understand condition setting linker 0x08003000 for KEIL compiler.

Does anyone help me explain condition 2 about Relocate vector table? How can we do that? Do we need modify in Compiler KEIL?

  
User program conditions
The user application to be loaded into the Flash memory using IAP should be built with the 
following configuration settings:
1. Set the program load address at 0x08003000, using the toolchain linker file.
2.  Relocate the vector table at address 0x20000000 (reserve 48 word starting in RAM @ 
0x20000000 ).

Outcomes