AnsweredAssumed Answered

STM32F405: Read 100% duty cycle

Question asked by marin on Sep 27, 2012
Latest reply on Sep 28, 2012 by David Littell
I am using STM32F405 in an application and in order to start working with the PWM module I have to check that I read a 100% duty cycle on one channel input.
I've been reading documentation, but it seems that input capture mode only works if there are transitions on the signal. This is not my case; I need to check that I read 100% duty cycle from the beginnning (input signal always to '1').

How can I do this? How should I configure the timer input?

Outcomes