AnsweredAssumed Answered

STM32F4 ADC1 starting conversion from TIM1 CC4 event - doesn't work

Question asked by petrovich.anatoly on Sep 23, 2012
Latest reply on Jun 11, 2014 by Chath :)
Hello. I colided with the following problem: ADC1 doesn't start conversion in injected channel from TIM1 CC4 event. Below I quote a piece of code of my initialization of ADC1 and TIM1:
RCC->APB2ENR|=RCC_APB2ENR_TIM1EN;  //TIM1 clocking enable
TIM1->PSC=83;                      //Prescaler 84 (83 + 1) (168 MHz/84=2 MHz)
TIM1->ARR=0xFFFF;                  //ARR value 
TIM1->CCER|=TIM_CCER_CC4E;         //Capture enable 4
TIM1->CCR4=10000;                  //CCR4 value
TIM1->CR1|=TIM_CR1_CEN;              //Counting enable
//****************************************************************
//*ADC1
//****************************************************************
void ADC_Config(void){
//------------------------------------------------------------------------------
//*GPIOA analog function
//------------------------------------------------------------------------------ 
RCC->AHB1ENR|=RCC_AHB1ENR_GPIOAEN; //PORTA clocking on
GPIOA->MODER|=GPIO_MODER_MODER1;   //PA1 analog function
//------------------------------------------------------------------------------
//*ADC1 initialization
//-----------------------------------------------------------------------------  
RCC->APB2ENR|=RCC_APB2ENR_ADC1EN; //ADC1 clocking on
ADC1->SMPR2|=ADC_SMPR2_SMP1_0
    |ADC_SMPR2_SMP1_1
    |ADC_SMPR2_SMP1_2;            //Conversion cycle
ADC1->JSQR|=ADC_JSQR_JSQ4_0;      //Conversion in which channel
//-------------------------------------------------------------------------------
ADC1->CR2&=~ADC_CR2_JEXTSEL;      //External event - TIM1_CH4
ADC1->CR2|=ADC_CR2_JEXTEN_0;      //Trigger detection on the rising edge
//-------------------------------------------------------------------------------
ADC1->CR2|=ADC_CR2_ADON;          //ADC1 ON
//ADC1->CR2|=ADC_CR2_JSWSTART;    //Starting conversion of injected channel
result=ADC1->JDR1;                //Result
}
I can't understand what and where I missed.

Outcomes