AnsweredAssumed Answered

Programing STM32F407 with the STM32VLDISCOVERY using SWD interface

Question asked by PA on Sep 21, 2012
Latest reply on Sep 22, 2012 by fm

Hi,

I'm trying to use the ST-Link on the STM32VLDISCOVERY board to program
a STM32F407ZGT6 using the SWD interface but it just don't work ...

I'm getting the "No target connect" error. I have triple checked all the connections,
the board is properly powered, ST-link drivers and Utility are the latest versions
(with support to the Z batch of the STM32F4).

I have used this same setup (St-Link on the STM32VLDISCOVERY) to successfully
program STM32F1 MCUs ... is there any technical reason for the ST link on the
STM32VLDISCOVERY not to recognise the STM32F407ZGT6 ?

Best regards,
PA

Outcomes