AnsweredAssumed Answered

LPS22HB calibration

Question asked by geisz.carl on Feb 11, 2016
Latest reply on Feb 22, 2016 by Muhuho.Adalberto
I am looking to increase the absolute accuracy of the LPS22 pressure reading.  It appears OPC can be set using registers 18h and 19h after soldering.  Can this give my an absolute altitude reading (at a small defined temp range) of +-0.1hPa without zero calibrating?  How do I reset the register using One Point Calibration?

Can the temperature be One Point Calibrated as well?

Outcomes