AnsweredAssumed Answered

To many elements in the array - stm32f103

Question asked by zbogar.dominik on Jul 27, 2012
Latest reply on Aug 4, 2012 by Andrew Neil
hello,

I have an issue. I'm using the stm32f103RB. When i want to create an array which has 8192 elements - const uint16_t table[8192] = {458,542...  }; The software successfully build in to the flash, but when i'm starting the debug mode, i get an error - "cannot access memmory" - error 57 or somethink. The program do not jump to the main. Than i change the array, which has less elements, aboute quarter of previous and the program normali works. I can not find the problem.. 

Outcomes