AnsweredAssumed Answered

stvp source code

Question asked by spectre on Jul 3, 2012
Latest reply on Jul 11, 2012 by laurent_l
Hi,

I need to force a reset on the stm32L32152 after the stvp programming session.
On the st site,there is the stvp source code and api example.
I saw the list of exported functions that may be called in EPRCORExx.DLL inside of the "PtkApi.cpp" ,but I don't find a function to force an mcu reset.

I need to force a reset on the nrst in order to exit from the programming mode,because the vdd of the mcu is connected to a supercap ,charged during the programming session via stvp.


Do I need to force a reset on the nrst pin manually ? Can I do it using the stvp api or something ?

regards

spectre

Outcomes