AnsweredAssumed Answered

configuration of DMA for DCMI

Question asked by matt on Jun 22, 2012
Latest reply on Jun 25, 2012 by matt

Hello,

I am trying to transfer image data from the DCMI data register via DMA to RAM memory. For this purpose I configure DMA2 as follows:

RCC_AHB2PeriphClockCmd(RCC_AHB1Periph_DMA2, ENABLE);

DMA_InitTypeDef   DMA_InitStruct;
 
DMA_DeInit(DMA2_Stream1);
 
DMA_StructInit(&DMA_InitStruct);
 
DMA_InitStruct.DMA_Channel            = DMA_Channel_1;
DMA_InitStruct.DMA_PeripheralBaseAddr = (uint32_t)(DCMI_BASE + 0x28);
DMA_InitStruct.DMA_Memory0BaseAddr    = (uint32_t)(&(Raw_Image_Data.Data[0]));
DMA_InitStruct.DMA_DIR                = DMA_DIR_PeripheralToMemory;
DMA_InitStruct.DMA_BufferSize         = 0xFFFF;
DMA_InitStruct.DMA_PeripheralInc      = DMA_PeripheralInc_Disable;
DMA_InitStruct.DMA_MemoryInc          = DMA_MemoryInc_Enable;
DMA_InitStruct.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Word; // word = 32 bit
DMA_InitStruct.DMA_MemoryDataSize     = DMA_MemoryDataSize_Word;     // word = 32 bit
DMA_InitStruct.DMA_Mode               = DMA_Mode_Normal;             // not circular
DMA_InitStruct.DMA_Priority           = DMA_Priority_Medium;
DMA_InitStruct.DMA_FIFOMode           = DMA_FIFOMode_Disable;        // direct mode
DMA_InitStruct.DMA_FIFOThreshold      = DMA_FIFOThreshold_Full;
DMA_InitStruct.DMA_MemoryBurst        = DMA_MemoryBurst_INC4;
DMA_InitStruct.DMA_PeripheralBurst    = DMA_PeripheralBurst_INC4;
   
DMA_Init(DMA2_Stream1, &DMA_InitStruct);
 
DMA_Cmd(DMA2_Stream1, ENABLE);

 

When I execute that code, the values in the register DMA2_S1CR do not change. Why?
Do I have to tell the DCMI somehow that it should connect with the DMA, e.g. using a similar command to SPI_I2S_DMACmd() ?

Please can anybody tell me what I am missing here?

Outcomes