AnsweredAssumed Answered

running application code after linux dfu-util load to flash ?

Question asked by adams.stuart on Jun 17, 2012
Latest reply on Jun 21, 2012 by Clive One
I am using dfu-util-0.6 under linux to load code to flash. After loading
to flash how do I get the STM32 to run the application code ? I tried
adding -R but the dfu device just re-enumerates after the USB reset.

Also oddly enough if I assert reset with BOOT0=0 without a power cycle
immediately after the DFU load, the application code does not run
(and neither does the DFU).
I have to actually power cycle the board to get the application to run from flash.
After that point a reset works to reset the application. (This happens on the STM32F107
eval board as well as our custom board.)

Outcomes