AnsweredAssumed Answered

TIM5 timer problem

Question asked by schneider.eli on Jun 10, 2012
Latest reply on Jul 11, 2012 by nikitin.vitaliy
There is a missing table in RM0090
para: 14.4.3 TIMx slave mode control register (TIMx_SMCR),
Table 60: TIMx internal trigger connection on page 395
I am trying to use TIM1 timer as a prescaler to TIM2 and TIM5 timers and this table is supposed to specify the ITRx signals routing for these timers. But, there is no table.

If you look to the rest of the page, there are missing bit descriptions too.

Eli

Outcomes