AnsweredAssumed Answered

Difference between AN3216 and stm32L-discovery board schematic

Question asked by spectre on May 28, 2012
Latest reply on May 30, 2012 by spectre
Hi,

I see on the an3216 "getting started with the stm32l hardware development" that there is a strange 10uF (ceramic?? non polarized ??) connected to the vdd.
Instead,if I see that on the stm32l discovery schematic the 10uF capacitor is not present.

Do I need to mount it or not ? 
Also,some one can tell me the value and the vendor code of the C26 1uF and of the L1  inductor on the stm32L-discovery board ?

regards,
Spectre






eaiiaafi.png

Outcomes