AnsweredAssumed Answered

Get and set feature reports with STM32_USB-FS-Device_Lib_V3.3.0?

Question asked by kipp.michael on May 27, 2012
Latest reply on Aug 21, 2015 by kipp.michael
Hello,

I'm working with STM32 since some weeks now and I'd like to use the Custom-Hid code from the STM32_USB-FS-Device_Lib_V3.3.0 for one of my projects based on STM32L151.

In contrary to the Custom-Hid example I'd like to use feature reports in addition to the input and output reports. In the example code feature reports are also defined, but I was not able to work with them.

I don't understand if, where and how they are processed with the given code. The host will work with HidD_GetFeature/HidD_SetFeature, but what about the device?

It would be great if someone had an idea that could help me.

Best regards and thanks in advance,
Michael

Outcomes