AnsweredAssumed Answered

STM32L152 TIM5

Question asked by shankland.brian on May 10, 2012
Latest reply on May 10, 2012 by shankland.brian
I have an interesting problem I hope someone can explain.

I was trying to modify the PWM_Input example from the StdPeriph examples to work with TIM5 so I could get a longer range. 

I have tried to use both TIM5_CH2 (PA1) and TIM5_CH4 (PA3) but on both occasions the input signal from my Agilent waveform generator SYNC output gets attenuated to 1.2V and no timer capture events occur.

If I switch to using TIM2 with the same pins the signal is not changed and the example works as expected.

Can anyone explain why I'm having this problem with using TIM5?

Outcomes