AnsweredAssumed Answered

5.7" TFT display 640X480 16bit FSMC part number

Question asked by ks.sk on May 8, 2012
Latest reply on May 10, 2012 by ks.sk

For my current project we are using a development board of powerAVR. It has a 3.5” TFT touchpanel with resolution 320x240, using 16bit FSMC bus for communication. But I need to have implement it on a 5.7” TFT with resolution 640x480.

We have been searching to find  a suitable part which is FSMC compatible, but with no success till now. can anyone provide the details regarding the part number of the same.

The controller on the development board is STM32F103ZE and the display controller is SSD1963. It will be very appreciated if the display controller is the same.

Outcomes