AnsweredAssumed Answered

First non-eval kit board help

Question asked by vonfange.gregory on Apr 23, 2012
Latest reply on Apr 24, 2012 by vonfange.gregory
Hi All,
I've been playing with a project on STM32VLDISCOVERY board for a while, and I'm trying to move it off eval board.  I wanted to start slow, so I ordered a LQFP-64 to DIP-64 SMT Adapter with the STM32F100RB soldered to it.  Using IAR Workbench and the Discovery as SWD Programmer, I get error whenever i try to connect saying "Fatal error: Failed to read CPUID for cortex device".
Anybody know what this means?  If I try to program the Discovery board directly it works fine.
Pins 19,32,48,64 connected to 3.3V
Pins 18,31,47,63 connect to GND
Pin 49 connected to SWCLK
Pin 46 connected to SWDIO
What am I missing?  Not even sure how to start debugging that error message?  Are there any examples of a very basic circuit that will just allow debugging?  I'm hoping to avoid external clock.  Is that possible?

Outcomes