AnsweredAssumed Answered

delay from two signals

Question asked by omede.marco on Apr 3, 2012
Latest reply on Apr 6, 2012 by omede.marco
Hello at all,
I have to mesaure the delay between 2 signals that I have in input to the microcontroller.

I saw the example of the PWM input.
I supposed to use an OR gate to have both front to the same pin but I think that there is a better solution using the timer in the microcontroller.

Can someone suggest a better idea using the timer to calculate the delay between two signal?
Many thanks for your help.
best regards.

Outcomes