AnsweredAssumed Answered

SysClock change during operation

Question asked by plasmaphase on Mar 20, 2012
Latest reply on Mar 24, 2012 by alokm
If there's another post which addresses my question, please direct me there.  I'm looking for a general idea as to how to change the system clock of the STM32F4 device while in operation.  I'd like to switch to a "low" power mode by reducing the clock down from 168MHz to, say, 2 MHz, and vice versa.  I'm pretty sure this requires me momentarily switching over to the internal oscillator or some other clock source to do so, but was just wondering if there was a firmware function call for this or if this was a bit more manual.  Any input is welcome.  Thanks in advance.

Outcomes