AnsweredAssumed Answered

STM32F217 & Ethernet PHY: KSZ8721BL & LwIp1.3.2 - ping trouble

Question asked by li.rayne on Mar 2, 2012
Latest reply on Mar 5, 2012 by li.rayne
Hello!
I have a board based on STM32F217.
Ethernet PHY: KSZ8721BL;
LwIp 1.3.2.
I took [url = "http://electronix.ru/redirect.php?http://www.st.com/internet/com/SOFTWARE_RESOURCES/SW_COMPONENT/FIRMWARE/stm32f2x7_eth_lwip.zip" ]this[/url] example of LwIp for STM32F2*7 and changed ethernet driver configuration for my board (change are highlighted):
stm32f2x7_eth_bsp.c
[b]#define CHECKSUM_BY_HARDWARE 1 [/b]
 
/*...................*/
 
void ETH_BSP_Config(void)
{
  /* Configure the GPIO ports for ethernet pins */
  ETH_GPIO_Config();
   
  /* Config NVIC for Ethernet */
  ETH_NVIC_Config();
 
  /* Configure the Ethernet MAC/DMA */
  ETH_MACDMA_Config();
[b]
/*  if (EthInitStatus == 0)
  {
    LCD_SetTextColor(Red);
    LCD_DisplayStringLine(Line5, (uint8_t*)"   Ethernet Init   ");
    LCD_DisplayStringLine(Line6, (uint8_t*)"      failed      ");
    while(1);
  }*/
 
  /* Configure the PHY to generate an interrupt on change of link status */
//  Eth_Link_PHYITConfig(DP83848_PHY_ADDRESS);
 
  /* Configure the EXTI for Ethernet link status. */
//  Eth_Link_EXTIConfig();[/b]
}
 
void ETH_GPIO_Config(void)
{
  GPIO_InitTypeDef GPIO_InitStructure;
 
  /* Enable GPIOs clocks */
  RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA | RCC_AHB1Periph_GPIOB |
                         RCC_AHB1Periph_GPIOC | RCC_AHB1Periph_GPIOI |
                         RCC_AHB1Periph_GPIOG | RCC_AHB1Periph_GPIOH |
                         RCC_AHB1Periph_GPIOF, ENABLE);
 
  /* Enable SYSCFG clock */
  RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE);
  
  /* Configure MCO (PA8) */
[b]  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8;
  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;
  GPIO_Init(GPIOA, &GPIO_InitStructure);[/b]
   
  /* MII/RMII Media interface selection --------------------------------------*/
#ifdef MII_MODE /* Mode MII with STM322xG-EVAL  */
 #ifdef PHY_CLOCK_MCO
 
  /* Output HSE clock (25MHz) on MCO pin (PA8) to clock the PHY */
  RCC_MCO1Config(RCC_MCO1Source_HSE, RCC_MCO1Div_1);
 #endif /* PHY_CLOCK_MCO */
 
  SYSCFG_ETH_MediaInterfaceConfig(SYSCFG_ETH_MediaInterface_MII);
#elif defined RMII_MODE  /* Mode RMII with STM322xG-EVAL *///!
 
  /* Output PLL clock divided by 2 (50MHz) on MCO pin (PA8) to clock the PHY */
  [b]RCC_MCO1Config(RCC_MCO1Source_PLLCLK, RCC_MCO1Div_2);[/b]
 
  SYSCFG_ETH_MediaInterfaceConfig(SYSCFG_ETH_MediaInterface_RMII);
[b]  SYSCFG_CompensationCellCmd(ENABLE);[/b]
#endif
   
  /* Configure PA1, PA2 and PA7 */
  GPIO_StructInit(&GPIO_InitStructure);
  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1;
  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
  GPIO_Init(GPIOA, &GPIO_InitStructure);
  GPIO_PinAFConfig(GPIOA, GPIO_PinSource1, GPIO_AF_ETH);
 
  GPIO_StructInit(&GPIO_InitStructure);
  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7;
  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
  GPIO_Init(GPIOA, &GPIO_InitStructure);
  GPIO_PinAFConfig(GPIOA, GPIO_PinSource7, GPIO_AF_ETH);
 
  GPIO_StructInit(&GPIO_InitStructure);
  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2;
  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
  GPIO_InitStructure.GPIO_OType = GPIO_OType_OD;
  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
  GPIO_Init(GPIOA, &GPIO_InitStructure);
  GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_ETH);
 
  /* Configure PC1, PC4 and PC5 */
  GPIO_StructInit(&GPIO_InitStructure);
  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4;
  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
  GPIO_Init(GPIOC, &GPIO_InitStructure);
  GPIO_PinAFConfig(GPIOC, GPIO_PinSource4, GPIO_AF_ETH);
 
  GPIO_StructInit(&GPIO_InitStructure);
  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5;
  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
  GPIO_Init(GPIOC, &GPIO_InitStructure);
  GPIO_PinAFConfig(GPIOC, GPIO_PinSource5, GPIO_AF_ETH);
 
  GPIO_StructInit(&GPIO_InitStructure);
  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1;
  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
  GPIO_Init(GPIOC, &GPIO_InitStructure);
  GPIO_PinAFConfig(GPIOC, GPIO_PinSource1, GPIO_AF_ETH);                               
 
  /* Configure PG14 and PG13 */
  GPIO_StructInit(&GPIO_InitStructure);
  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_13 | GPIO_Pin_14;
  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
  GPIO_Init(GPIOG, &GPIO_InitStructure);
  GPIO_PinAFConfig(GPIOG, GPIO_PinSource13, GPIO_AF_ETH);
  GPIO_PinAFConfig(GPIOG, GPIO_PinSource14, GPIO_AF_ETH);
 
    /* Configure PB11 */   
[b]  GPIO_StructInit(&GPIO_InitStructure);
  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11;
  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
  GPIO_Init(GPIOB, &GPIO_InitStructure);
  GPIO_PinAFConfig(GPIOB, GPIO_PinSource11, GPIO_AF_ETH);[/b]
 
}
system_stm32f2xx.c:
uint32_t SystemCoreClock = 100000000;

The board started working with this code successfully.
After 2-4 hour the board ceased to answer.

Interesting fact:
At the start of pinging the responce time <= 1 ms.
After some time (always random period) pinging changes to 400-2000ms.
If I start  pinging on a second computer  with option -f(flood), pings to board will change to 1-40ms.
After stop pinging on the second computer the responce time returns to 400-2000ms again.

Somebody met this problem?
Regards, Rayne.

Outcomes