AnsweredAssumed Answered

VL6180X

Question asked by burke.dave on Apr 21, 2015
Latest reply on Sep 26, 2016 by Chatouri.Manuel
Hi

I'm just bringing up a VL6180x mounted on a VL6180X-Satellite board with bit banging software. Everything has gone well so far, writing and reading registers etc, for proximity only application. The ranging output goes to a minimum of 18 at 100mm and shows a system error of 2? reading the RESULT__RANGE_STATUS register.

I found the AN4545 with the private register writes but this seems to differ slightly to one of your earlier replies to other queries? You have extra register writes! Is there a further update to this list.

Also I'm interested in being able to detect approach up to 400mm away and then going to fine approach as the device nears the target. Is this possible?

Regards
Dave B

Outcomes