AnsweredAssumed Answered

Clock for ULPI PHY?

Question asked by singer.marc on Feb 16, 2012
Latest reply on Feb 16, 2012 by Clive One
Greetings,

We're having a hard time telling whether or not the STM32F207 will drive the clock for the PHY.  There is a sentence in the datasheet that says, vaguely

   External HS or HS OTG operation supporting ULPI in SDR mode. The OTG PHY is
connected to the microcontroller ULPI port through 12 signals. It can be clocked using
the 60 MHz output.

Does this mean we have to use one of the MCO outputs?  Or will the ULPI clock be driven at 60MHz?

Outcomes