AnsweredAssumed Answered

STM32F2xx USB Library - Default COM Port Configuration

Question asked by hansen.terry on Feb 15, 2012
Latest reply on Feb 15, 2012 by hansen.terry
I am trying to use the VCP example project in the STM32F2xx USB library on an IAR STM32F207 dev board.

The device enumerates correctly when I plug in a laptop and it is recognized by the ST VCP USB driver as COM4.  But it looks like the USB library's default configuration for the UART in the VCP project (in file usbd_cdc_vcp.c) is 8O1, ie odd parity.  Also, when the VCP enumerates on the laptop, it sends a SET_LINE_CODING message back to the library that configures the UART as 8O1.  (The HyperTerminal on the laptop attached to the VCP is set to 8N1.)  None of my existing comms will work with 8O1.  Is there a way to make the VCP driver on the laptop switch to 8N1?

Also, I am reluctant to modify the USB library code from a default of 8O1 to 8N1 without understanding why it is set to 8O1.  From my experience, 8O1 is kind of unusual and 8N1 is more normal.  Is there a reason for choosing 8O1?  And if so, am I going to mess something up by modifying the code to do 8N1?

Thanks in advance!

Outcomes