AnsweredAssumed Answered

Timer1 trigger for ADC2

Question asked by Franz Wegerer on Feb 10, 2012
Latest reply on Feb 10, 2012 by baird.hal.001
Hi,

Using STM32F205RCT6.
We used ADC1/DMA with Timer 1 as trigger and worked fine. The temperature sensor is only connected to ADC1 so I have to move ADC1 -> ADC2. Now we have problems with the trigger - it doesn't work anymore.
http://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/REFERENCE_MANUAL/CD00225773.pdf
Figure 35. Multi ADC block diagram

Are the trigger signals connect to the slaves when independent mode is selected? I can't find any information about that.

Any ideas would be most welcome.
Thanks

Outcomes